earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Specifications

Specifications


Products: Enterprise Central
Functionalities: Engineering
1/28/2026

Enterprise Central

arrow1_rotationIntroduction arrow1_rotationFeatures arrow1_rotationSpecifications
 
action_zoom_plus_stroke Enterprise Central
Figure: Enterprise Central

Introduction

EcoStruxure Building Operation Enterprise Central is the top-tier EcoStruxure BMS server in a large Building Management System and is intended for system specific tasks and supervision. Enterprise Central can host several Enterprise Servers, which in turn can host multiple field servers. As the dedicated server at the top of the system architecture hierarchy, Enterprise Central provides an entry point from which you can configure, control, monitor, and search the entire system. Enterprise Central collects site-wide data for aggregation and archiving and serves as a single point of administration through WorkStation or WebStation.

For Corporate Facility Managers, Senior Engineering Managers, Chief Space Planners and others who need to manage their buildings in a global, aggregated, and efficient manner, Enterprise Central is an EcoStruxure BMS server that allows users to scale operations management across the largest buildings, campuses, and multi-site corporate real estate portfolios from a single location by generating aggregated reports, standardizing critical security policies, normalizing alarm presentation and prioritization, and auditing activity across the entire organization.

Unlike other BMSs which focus on a single location or on a single aspect of the operation, Enterprise Central provides a single pane of glass across all aspects of a large real estate portfolio.

Features

Enterprise Central has the following main features:

  • Global view, access, and search of the system

  • Centralized alarms and data management:

    • Alarms from multiple servers

    • Event logs from multiple servers

    • Extended trend logs from multiple servers

    • Historical data storage from multiple servers

  • Scalability

  • User and domain management

  • Windows Active Directory integration

Semantic

Enterprise Server and Enterprise Central come with built-in support for modelling of the “digital twin” of the building, site, campus, and region using Brick Schema. WorkStation and WebStation provide enhanced human understandability through the additional context that is given to alarms and points through the “digital twin”. The required graph database is included in the installation packages. WorkStation can be used to create the model, or it can be imported using the graph database user interface.

Global view, access, and search of the system

The entire system, including all mid-tier Enterprise Servers and the base-tier field servers with their associated Central IO modules, field controllers, and other field devices, can be accessed and configured through Enterprise Central. When logged on to Enterprise Central, you can also search the entire system, and view alarm and event data from all associated Enterprise Servers and field servers. In short, with the exception of not hosting its own layer of field bus devices, Enterprise Central carries the same full feature set as the Enterprise Servers.

Centralized alarms and data management

Alarms from the Enterprise Servers, field servers, and their associated devices throughout the site, are collected by Enterprise Central for centralized logging, display, and management. Alarms can trigger email, SNMP, file, or client notifications, which can include alarm, point value, or trend log data. Notifications can also be triggered periodically by schedules or other binary values.

Users can also view event logs and trend logs from multiple Enterprise Servers and field servers. The historical event data is collected from the multiple servers and stored in a central database.

EcoStruxure BMS servers can be configured to automatically store all historical data, trend log data, event log and audit trail data, in an external database. If data needs to be available for longer periods of time, an external log storage can be incorporated into the EcoStruxure BMS without the need for extensive engineering work. The supported databases are TimescaleDB, which is built on PostgreSQL, and Microsoft SQL Server. The data in the external log storage is available natively to the viewers built into the EcoStruxure Building Operation clients and to the built-in reporting functionality.

You can use the powerful Log Processor functionality for custom processing of trend data for viewing in charts, dashboards and for inclusion in reports. The Log Processor enables advanced calculations on one or multiple trend logs and point values.

Examples of advanced calculations:

  • Energy usage normalization

  • Virtual submeters and summaries

  • Calculation of Mean Kinetic Temperature

  • Unit conversions

  • Average, maximum, and mini m um over custom periods

The output of the Log Processor can be saved in the database, including the External Log Storage or calculated automatically on demand.

Selected trend logs and the event log can be sent to AVEVA PI System directly without the need for intermediate storage or specialized PI System connectors.

User and domain management

You can use Enterprise Central to create and configure domains, user groups, and permissions.

Reporting

The EcoStruxure BMS servers provide built-in functionality for basic reporting that can deliver reports in any text format and XLSX, without any dependencies to other external software. Reports for XLSX can be enriched by using advanced functionality such as formulas, conditional formatting, charts and sparklines.

Reports can be generated on schedule, on an alarm event or other custom conditions, and you can get the output delivered via email or written to file.

Using Enterprise Server and Enterprise Central, reports can be converted to PDF, and you can elevate the data security and traceability even further by using the optional add-on for automatically signing PDF reports with a digital certificate upon generation. This validates that the content has not been altered after the report was generated.

Authentication and permissions

An EcoStruxure BMS provides a powerful permission system that is easy to manage, flexible, and adapts to all kinds of system sizes. The permission system provides a high standard of authentication. Authentication is done against the built-in user account management system , against Windows Active Directory Domains , or via SAML 2.0 single sign-on . The built-in account management system allows an administrator to establish password policies that meet stringent cybersecurity guidelines. When Windows Active Directory or SAML 2.0 authentication is used, the administration costs are lower because users do not have to be managed in multiple directories.

With Enterprise Central, the password policies are standardized across all hosted Enterprise Servers.

Advanced activity log

It is important to log more than basic activity. In an EcoStruxure BMS, every action is logged with a timestamp, the user who performed the action, and the values that were changed.

WorkStation/WebStation interface

Through any client, the user experience is similar regardless of which EcoStruxure BMS server the user is logged on to. The user can log directly on to an Enterprise Central to commission, supervise, and monitor the Enterprise Servers and field servers with their attached Central IO modules, field controllers, and other field devices. For more information, see the WorkStation and WebStation specification sheets.

Web Services support

Enterprise Central supports the use of Web Services based on open standards, such as SOAP and REST, to consume data into the EcoStruxure BMS. Use incoming third-party data (temperature forecast, energy cost) over the Web to determine site modes, scheduling, and programming.

EcoStruxure Web Services support

EcoStruxure Web Services, Schneider Electric’s Web Services standard, is natively supported in the EcoStruxure BMS servers. EcoStruxure Web Services offers extra features between compliant systems whether within Schneider Electric or other authorized systems. These features include access to semantic model, system directory browsing, read/write of current values, alarm receipt and acknowledgement, and historical trend log data. EcoStruxure Web Services requires user name and password to log on to the system.

IT friendly

The EcoStruxure BMS servers communicate using the networking standards. This makes installations easy, management simple, and transactions encrypted for protection.

Supported Protocols
  • IP addressing

  • TCP communications

  • DHCP for easy network configuration

  • DNS for simple lookup of addresses

  • HTTP/HTTPS for internet access through firewalls, which enables remote monitoring and control

  • NTP (Network Time Protocol) for time synchronization throughout the system

  • SMTP or SMTPS with support for SSL/TLS based authentication, enables sending email messages triggered by schedule or alarm

  • SNMP enables reception of application alarms in designated network management tools

TLS support

Communication between clients and the EcoStruxure BMS servers , and between EcoStruxure BMS servers, can be encrypted using Transport Layer Security (TLS ). The servers are delivered with a default self-signed certificate. Commercial Certification Authority (CA) server certificates are supported to lower the risk of malicious information technology attacks. Use of encrypted communication can be enforced for both WorkStation and WebStation access.

Table: Building Automation – Windows and Linux Licences Availablility

Enterprise Central Licenses

Windows

Linux

Enterprise Central - 2 Enterprise Servers a

Yes

Yes

Enterprise Central - 5 Enterprise Servers a

Yes

Yes

Enterprise Central - 10 Enterprise Servers a

Yes

Yes

  1. For more information on the part numbers, see section “Specifications”, subsection “Part Numbers”.

Upgrade Software Bundle Licences

Windows

Linux

Upgrade 3.x - 5 Enterprise Servers a

Yes

-

Upgrade 3.x - 10 Enterprise Servers a

Yes

-

Upgrade 4.x or 5.x - 5 Enterprise Servers a

Yes

-

Upgrade 4.x or 5.x - 10 Enterprise Servers a

Yes

-

  1. For more information on the upgrade software bundles, see section “Specifications”, subsection “Upgrade software bundles”.

Add-on Option Licences

Windows

Linux

EC Hosting Pack - 3 a

Yes

Yes

EC Hosting Pack - 5 a

Yes

Yes

EcoStruxure Web Services Consume a

Yes

Yes

EcoStruxure Web Services Serve & Consume a

Yes

Yes

EcoStruxure Web Services Serve & Consume and Historical trend log data a

Yes

Yes

Web Services (Generic Consume) option a

Yes

Yes

Alarm notifications via SNMP option a

Yes

Yes

Personal Dashboards option a

Yes

Yes

TimescaleDB connection option a

Yes

Yes

Microsoft SQL Server connection option a

Yes

Yes

AVEVA PI System connection option a

Yes

Yes

Regulated Industries Compliance Pack option a

Yes

Yes

PDF signing option a

Yes

Yes

SAML Authentication option a

Yes

Yes

Semantic DB Plus 2 CPU Cores a

Yes

-

Semantic DB Plus 6 CPU Cores a

Yes

-

Semantic DB External Use Plus 2 CPU Cores a

Yes

-

Semantic DB External Use Plus 6 CPU Cores a

Yes

-

Sustainability Pack option a

Yes

Yes

  1. For more information on the add-on options, see section “Specifications”, subsection “Add-on options”.

Table: Fire Detection – Windows and Linux Licences Availablility

Enterprise Central Licenses

Windows

Linux

Enterprise Central 1 year on premise subscription duration a

Yes

-

  1. For more information on the part numbers, see section “Specifications”, subsection “Part Numbers”.

Specifications

Hardware requirements
Processor power, memory, and storage capacity should be scaled upwards to accommodate targeted system size as impacted by the total quantity of Enterprise Servers, automation servers, and expected historical archiving. Enterprise Central is tested on a server with an 8-core 3.6 GHz processor, a 16 GB of memory, and an SSD storage capacity of 4 TB.
Processor
Minimum: Intel Core i5 @ 3.0 GHz, or another x86-64 processor with comparable performance
  
Recommended: Intel Core i5 @ 4.0 GHz or better
Memory
Minimum: 8 GB
  
Recommended: 16 GB or higher
Storage capacity
Minimum: 1 TB
  
Recommended: 4 TB
Storage device
Recommended: Enterprise Solid State Drive (SSD)
An Enterprise SSD is recommended to maintain the necessary speed and stability. The database and the binaries should both be installed on the Enterprise SSD.
Other devices
Microsoft mouse or compatible pointing device is required.
Software requirements
Operating systems – Enterprise Central for Windows
Microsoft Windows 10 (64-bit)
  
Microsoft Windows 11 a
  
Microsoft Windows Server 2012 R2 (64-bit)
  
Microsoft Windows Server 2016
  
Microsoft Windows Server 2019
  
Microsoft Windows Server 2022 a
The following Microsoft Windows 10 editions are supported: Pro and Enterprise.
The following Microsoft Windows 11 a editions are supported: Pro and Enterprise.
The following Microsoft Windows Server 2012 R2 editions are supported: Datacenter, Standard, Essentials, and Foundation.
The following Microsoft Windows Server 2016 editions are supported: Datacenter, Standard, and Essentials.
The following Microsoft Windows Server 2019 editions are supported: Datacenter, Standard, and Essentials.
The following Microsoft Windows Server 2022 a editions are supported: Datacenter, Standard, and Essentials.
Operating systems – Enterprise Central for Linux
OCI compliant container runtime on Linux x86-64
Quality assurance testing has been performed on, and support is provided with, Ubuntu 20.04 and 22.04 with Docker Engine. Other deployment scenarios have not been tested by Schneider Electric. Product Support Services may require that potential issues can be reproduced in tested and supported environment for full support.
Required additional software – Enterprise Central for Windows
Microsoft .NET Framework 4.7.2 and later
The Microsoft .NET Framework is required by Software Administrator.
External log storage PostgreSQL option
Supported versions of PostgreSQL ( www.postgresql.org ) with matching version of TimescaleDB extension ( www.timescale.com ).
  
Note: To use compression for trend data, TimescaleDB 2.11 or later is required.
Quality assurance testing has been performed by Schneider Electric with TimescaleDB and PostgreSQL installed natively in Windows 10, Windows Server 2012, 2016, and 2019. Other deployment scenarios have not been tested by Schneider Electric.
External log storage Microsoft SQL option
Microsoft SQL Server versions under full support by Microsoft ( www.microsoft.com ).
The following Microsoft SQL Server editions are supported: Enterprise, Standard, and Express.
External log storage AVEVA PI System option
PI Web API 2021 SP3 and database compatible with that version
Quality assurance testing has been performed by Schneider Electric with PI Web API 2021 SP3, and database compatible with that version, installed on Windows Server 2019. Other deployment scenarios have not been tested by Schneider Electric.
Communication
TCP
Binary, port fixed, 4444
HTTP
Non-binary, port configurable, default 80
HTTPS
Encrypted supporting TLS 1.3, 1.2, 1.1 a , and 1.0 a , port configurable default 443
SMTP
Email sending, port configurable, default 25
SMTPS
Email sending, port configurable, default 587
SNMP
version 3
  
Application alarm distribution using trap
NTP
Time synchronization
Part numbers
Building Automation – Enterprise Central for Windows
Enterprise Central - 2 , EcoStruxure Building Operation Enterprise Central license for a PC server, includes support to 2 Enterprise Servers , 3 concurrent clients , and 1 semantic database limited to 2 CPU cores
SXWSWECXX00002
Enterprise Central - 5, EcoStruxure Building Operation Enterprise Central license for a PC server, includes support to 5 Enterprise Servers , 3 concurrent clients , and 1 semantic database limited to 2 CPU cores
SXWSWECXX00005
Enterprise Central - 10, EcoStruxure Building Operation Enterprise Central license for a PC server, includes support to 10 Enterprise Servers , 3 concurrent clients , and 1 semantic database limited to 2 CPU cores
SXWSWECXX00010
Building Automation – Enterprise Central for Linux
Enterprise Central - 2, EcoStruxure Building Operation Enterprise Central for Linux license for a PC server, includes support to 2 Enterprise Servers and 3 concurrent clients
SXWSWECLX00002
Enterprise Central - 5, EcoStruxure Building Operation Enterprise Central for Linux license for a PC server, includes support to 5 Enterprise Servers and 3 concurrent clients
SXWSWECLX00005
Enterprise Central - 10, EcoStruxure Building Operation Enterprise Central for Linux license for a PC server, includes support to 10 Enterprise Servers and 3 concurrent clients
SXWSWECLX00010
Fire Detection – Enterprise Central for Windows
Enterprise Central 1 year on premise subscription duration
FFSEFOSEC00012
Upgrade software bundles
Building Automation – Enterprise Central for Windows
Enterprise Central Upgrade – 5 or fewer Enterprise Servers
Upgrades Enterprise Central, with 5 or fewer hosted Enterprise Servers, from EcoStruxure Building Operation software version 3.x to 6.0.
SXWSWECUP30005
Enterprise Central Upgrade – 10 or fewer Enterprise Servers
Upgrades Enterprise Central, with 10 or fewer hosted Enterprise Servers, from EcoStruxure Building Operation software version 3.x to 6.0.
SXWSWECUP30010
Enterprise Central Upgrade – 2 or fewer Enterprise Servers
Upgrades Enterprise Central, with 2 or fewer hosted Enterprise Servers, from EcoStruxure Building Operation software version 4.x or 5.x to 6.0.
SXWSWECUP40002
Enterprise Central Upgrade – 5 or fewer Enterprise Servers
Upgrades Enterprise Central, with 5 or fewer hosted Enterprise Servers, from EcoStruxure Building Operation software version 4.x or 5.x to 6.0.
SXWSWECUP40005
Enterprise Central Upgrade – 10 or fewer Enterprise Servers
Upgrades Enterprise Central, with 10 or fewer hosted Enterprise Servers, from EcoStruxure Building Operation software version 4.x or 5.x to 6.0.
SXWSWECUP40010
Add-on options
Building Automation – Enterprise Central for Windows
EC Hosting Pack -3, License to add 3 Enterprise Servers
in addition to the original Enterprise Central purchased size
SXWSWESEC00003
EC Hosting Pack -5, License to add 5 Enterprise Servers
in addition to the original Enterprise Central purchased size
SXWSWESEC00005
SW-EWS-1, EcoStruxure Web Services (run-time) option
Consume only for one Enterprise Server or one Enterprise Central
SXWSWEWSX00001
SW-EWS-2, EcoStruxure Web Services (run-time) option
Serve & Consume for one Enterprise Server or one Enterprise Central
SXWSWEWSX00002
SW-EWS-3, EcoStruxure Web Services (run-time) option
Serve & Consume, plus Historical trend log data for one Enterprise Server or one Enterprise Central
SXWSWEWSX00003
SW-GWS-1, Web Services (Generic Consume) option
For one Enterprise Server or one Enterprise Central
SXWSWGWSX00001
SW-SNMP-1, Alarm notifications via SNMP option
For one Enterprise Server or one Enterprise Central
SXWSWSNMP00001
Building Operation Personal Dashboards option, 1 per server required for users logging on to that server to have Personal Dashboard capabilities
For one Enterprise Server or one Enterprise Central
SXWSWDASH00001
SW-ECDBTS-1, TimescaleDB connection option
For one Enterprise Central
SXWSWECDBTS001
EcoStruxure Building Operation, Microsoft SQL Server connection option
For one Enterprise Central
SXWSWECDBMS001
EcoStruxure Building Operation, AVEVA PI System connection option
For one Enterprise Central
SXWSWECDBPI001
Regulated Industries Compliance Pack option
For one Enterprise Server or one Enterprise Central
SXWSWCMPLPK001*
SW-ECPDF-1, Building Operation PDF signing option
For one Enterprise Central
SXWSWECPDFSS01
SAML Authentication option
For one Enterprise Central
SXWSWECSAML001
Semantic DB Plus 2 CPU Cores
Additional concurrent queries for one semantic database
SXWSWSTDBAC002
Semantic DB Plus 6 CPU Cores
Additional concurrent queries for one semantic database
SXWSWSTDBAC006
Semantic DB External Use Plus 2 CPU Cores
Enables queries from external tools and additional concurrent queries
SXWSWSTDBEUAC2
Semantic DB External Use Plus 6 CPU Cores
Enables queries from external tools and additional concurrent queries
SXWSWSTDBEUAC6
Sustainability Pack option
For one Enterprise Central for Windows
SXWSWECSUSPKW1
Building Automation – Enterprise Central for Linux
EC Hosting Pack - 3, License to add 3 Enterprise Servers
in addition to the original Enterprise Central for Linux purchased size
SXWSWESECL0003
EC Hosting Pack - 5, License to add 5 Enterprise Servers
in addition to the original Enterprise Central for Linux purchased size
SXWSWESECL0005
EcoStruxure Web Services (run-time) option
Consume only for one Enterprise Server for Linux or one Enterprise Central for Linux
SXWSWEWSL00001
EcoStruxure Web Services (run-time) option
Serve & Consume for one Enterprise Server for Linux or one Enterprise Central for Linux
SXWSWEWSL00002
EcoStruxure Web Services (run-time) option
Serve & Consume, plus Historical trend log data for one Enterprise Server for Linux or one Enterprise Central for Linux
SXWSWEWSL00003
Web Services (Generic Consume) option
For one Enterprise Server for Linux or one Enterprise Central for Linux
SXWSWGWSL00001
Alarm notifications via SNMP option
For one Enterprise Server for Linux or one Enterprise Central for Linux
SXWSWSNMPL0001
Personal Dashboards option, 1 per server required for users logging on to that server to have Personal Dashboard capabilities
For one Enterprise Server for Linux or one Enterprise Central for Linux
SXWSWDASHL0001
TimescaleDB connection option
For one Enterprise Central for Linux
SXWSWECDBTSL01
Microsoft SQL Server connection option
For one Enterprise Central for Linux
SXWSWECDBMSL01
AVEVA PI System connection option
For one Enterprise Central for Linux
SXWSWECDBPIL01
Regulated Industries Compliance Pack option
For one Enterprise Server for Linux or one Enterprise Central for Linux
SXWSWCMPLPKL01*
PDF signing option
For one Enterprise Central for Linux
SXWSWECPDFSSL1
SAML Authentication option
For one Enterprise Central for Linux
SXWSWECSAMLL01
Sustainability Pack option
For one Enterprise Central for Linux
SXWSWECSUSPKL1