earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WorkStation
Functionalities: Schedules
10/30/2025

Schedule Settings Dialog Box

Use the Schedule Settings dialog box to edit the configuration settings for the selected schedule.

 
action_zoom_plus_stroke Schedule settings dialog box
Figure: Schedule settings dialog box

Table: Schedule Settings Dialog Box

Component

Description

Remove past events

Select True to remove events that have already occurred from the selected schedule.

Lead object

Click to select a lead schedule if you want the selected schedule to be a shadow schedule. For more information, see Lead and Shadow Relationship .

Default value

Enter a default value for the selected schedule.

Description

Type a description for the selected schedule.

  • Lead and Shadow Relationship
  • Schedule Workspace Toolbar