earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: User Management
10/30/2025

Relative Path Permissions Rules

You set permissions on a relative path twice.

First, you set permissions on the objects in the template. Objects in the template can be granted the following path permissions: Read, Write, Create, Delete, Edit, Force and Command.

Second, you set permissions for user accounts and user account groups. A user account or a user account group can be granted the following path permissions: Read, Write, Create, Delete, Edit, Force and Command.

Table: Software Permissions Rules

Property

Description

Read

Permits viewing and listing path content

Write

Permits an administrator to change configurations except for bindings, programs, and graphics

Create

Permits creating new objects on the path

Delete

Permits deleting objects under the path. Delete permissions are required on a folder to delete its contents

Edit

Permits editing objects on the path

Force

Permits forcing values on the path

Command

Permits the execution of commands on the path. Command permissions can override this permission for specific commands

Inherited

Indicates that the permissions are inherited from the parent folder

Note:

You need delete permissions to rename, paste and duplicate folders and objects in EcoStruxure Building Operation software.

Note:

You can always edit graphic and program objects in the relevant editor, however in order to save it on your server you need "Edit" permissions. You can save your edits on your hard drive or export to a location of your choice even if you don’t have “Edit” permissions.

  • Relative Path Permissions