earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: User Management
10/30/2025

Editing Type Permissions Templates

You edit type permissions template to change permissions to this type.

Show More
action_close

You set permissions on a type twice.

First, you set permissions on the type of object. Types can be granted the following path permissions: Read, Write, Create, Delete, Edit, Force, Command and Inherited. You need to assign at least Read permissions on the type.

Second, you set permissions for user accounts and user account groups. A user account or a user account group can be granted or refused permissions to the type.

Table: Software Permissions Rules

Property

Description

Read

Permits viewing and listing path content

Write

Permits an administrator to change configurations except for bindings, programs, and graphics

Create

Permits creating new objects on the path

Delete

Permits deleting objects under the path. Delete permissions are required on a folder to delete its contents

Edit

Permits editing objects on the path

Force

Permits forcing values on the path

Command

Permits the execution of commands on the path. Command permissions can override this permission for specific commands

Inherited

Indicates that the permissions are inherited from the parent folder

Note:

You need delete permissions to rename, paste and duplicate folders and objects in EcoStruxure Building Operation software.

Note:

You can always edit graphic and program objects in the relevant editor, however in order to save it on your server you need "Edit" permissions. You can save your edits on your hard drive or export to a location of your choice even if you don’t have “Edit” permissions.

To edit a type permissions template
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Type permissions .

  4. In the System Tree pane, select the type permissions you want to edit.

  5. In the Relative object list, choose the object you want to edit.

  6. In the rules table, choose permissions for the type.

  7. Click the Save button

     
    action_zoom_plus_stroke
    .

A user account or a user account group is now granted a new set of permissions for a given type.

  • Type Permissions Rules
  • Software Permissions Rules Management
  • Creating Type Permissions Templates
  • Removing Path Permissions Templates
  • Removing Type Permissions from User Accounts or User Account Groups
  • Assigning Type Permissions to User Accounts or User Account Groups