earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Dashboards
12/2/2024

Period over Period Chart Properties – Dialog Box

Use the Period over Period Chart Properties dialog box to configure and edit a period over period chart.

 
action_zoom_plus_stroke Period over period chart properties dialog box
Figure: Period over period chart properties dialog box

Table: Period over Period Chart Properties Dialog Box

Component

Description

Add

Click to add a trend log.

Display trend log

Enter the trend log you want to display.

Chart type

Select the type of chart you want to display.

Calculation method

Select the calculation method for the trend log. For more information, see Calculation Methods .

Color

Select the color you want to use for the trend log.

Y-axis

Select the position of the y-axis.

Missing data

Select how to display missing data.

Period

Select the period you want to display.

Caption

Type a caption for the widget.

Caption Link

Select to make a link to an object that is relevant to the values that are displayed in the widget.

Show Legend

Click True to display the name and color of the trend log in the widget.

Show Period

Select to display the period as a legend.

Stack series

Select to stack the series.

Y-axis minimum

Enter the Y-axis minimum.

Y-axis maximum

Enter the Y-axis maximum.

Decimals

Select the number of decimals you want to display.

  • Dashboard Widgets
  • Period over Period Chart
  • Widget Dialog Box – Layout Tab