earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Dashboards
10/30/2025

Adding a Graphic to a Dashboard

You add graphics to a dashboard to enhance the overview.

Show More
action_close

Graphics can be added to a dashboard.

When you add a graphic to a dashboard, the graphic keeps all of its functions. For example, links in the graphics to other objects work and values in the graphics can be changed and forced.

The graphics that are already in the Select Dashboard Widgets dialog box are custom types. They are visible in the Custom Types Library in WorkStation. When you add a graphic already in the Select Dashboard Widgets dialog box the graphic is an instance of the custom type.

To adding a graphic to a dashboard
  1. In WebStation, right-click the dashboard.

  2. Click Edit Dashboard .

  3. Click Add and do one of the following:

    • Select a graphic in the Select dashboard widgets dialog box.

    • Click Browse and select a graphic.

  4. Click OK .

  • Dashboard Widgets
  • Graphics in Dashboards
  • Select Dashboard Widgets Dialog Box
  • Dashboard Widgets Toolbar