earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Dashboards
10/30/2025

Dashboard Properties – Basic Tab

Use the Dashboard Properties dialog box to configure a dashboard.

 
action_zoom_plus_stroke Dashboard Properties – Basic tab
Figure: Dashboard Properties – Basic tab

Table: Dashboard Properties – Basic Tab

Component

Description

Caption

Type a caption for the dashboard.

Show date and time

Select True to display the server date and time in the upper right corner of the dashboard.

Background color

Enter a background color.

Background image

Select a background image.

The background image must already exist in your EcoStruxure Building Operation system. If not, you add the background image as a document.

For more information, see Documents Overview .

Blur background

Select True to blur the background image. This will blur the background of widgets if the widget opacity is below 100%.

Opacity

Select the opacity on the widgets.

  • How Dashboards Work
  • Documents Overview