earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Device Administrator, FDP Server, License Administrator
Functionalities: License Management
11/15/2025

Field Server Licensing Overview

Device Administrator is used to manage licenses on field servers.

Software and Features that Require Licenses

A number of software and features need licenses.

For more information, see Software and Features that Require Licenses .

Entitlements, Products, and Licenses

Licenses are bought as products and delivered in Entitlements. An Entitlement is a container that can contain several products. The products contain the licenses and they can differ in quantity and contents.

Field Server Licensing Workflow

Use one of these workflows, depending on if the field servers are connected or not connected to the Internet.

For more information, see Automation Server Licensing on Automation Servers not Connected to Internet Workflow .

Certificates

It is recommended to use HTTPS for the communication between Device Administrator and field servers when you manage licenses.

For more information, see Certificates in Device Administrator .

Return Licenses on Field Servers

You can return licenses from field servers.

For more information, see Return Licenses on Field Servers .

  • Software and Features that Require Licenses
  • Inherited Licenses
  • Automation Server Licensing on Automation Servers not Connected to Internet Workflow
  • Certificates in Device Administrator
  • Return Licenses on Field Servers