earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Dashboards
12/2/2024

Log Pie Properties Dialog Box

Use the Log Pie Properties dialog box to configure and edit a log pie.

 
action_zoom_plus_stroke Log pie properties dialog box
Figure: Log pie properties dialog box

Table: Log Pie Properties Dialog Box

Component

Description

Add

Click to add a trend log.

Display trend log

Enter the trend log you want to display.

Calculation method

Select the calculation method for the trend log. For more information, see Calculation Methods .

Color

Select the color for the trend log.

Period

Select the period you want to display.

Caption

Type a caption for the widget.

Caption Link

Select to make a link to an object that is relevant to the values that are displayed in the widget.

Pie Center

Select how you want to display the pie center.

For more information, see Log Pie .

Show Legend

Click True to display the name and color of the trend log in the widget.

Show Percentage

Select to display the values in percentage.

Show Period

Select to display the period as a legend.

  • Dashboard Widgets
  • Log Pie
  • Widget Dialog Box – Layout Tab