earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Device Administrator, FDP Server, ​License Administrator
Functionalities: Engineering
3/6/2025

Centralized Licensing on EcoStruxure BMS Servers Connected to Internet Workflow

Use this workflow to add licenses to EcoStruxure BMS servers with access to Internet.

Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke EcoStruxure BMS server licensing workflow
Figure: EcoStruxure BMS server licensing workflow
Install certificates on the EcoStruxure BMS server

Install certificates if you use HTTPS for communication.

For more information, see Device Administrator Certificate Workflow .

Entitlements

Make sure that you have the Entitlements containing the licenses. You need the email with the entitlement during the process.

Make sure that the EcoStruxure BMS server have access to Internet

The EcoStruxure BMS server must have access to Internet for the activation process.

For more information, see Information Technology System Planning Guide .

Add an entitlement in Device Administrator

In Device Administrator, you add entitlements that contains products and licenses.

This is done so that you can view all licenses that are available to be assigned and then activated.

Make sure that you have the HTML entitlement certificate file or the entitlement ID available .

There are two different procedures to add and set up an entitlement when you have a EcoStruxure BMS server connected to internet:

Assign licenses to the EcoStruxure BMS server

Use the License Products available in the entitlements to assign License Features to the EcoStruxure BMS servers.

For more information, see Assigning Licenses .

Activate licenses onthe EcoStruxure BMS server

For more information, see Activating Licenses Online .

  • Centralized Licensing Overview
  • Information Technology System Planning Guide
  • Adding an Entitlement using the HTML file when an EcoStruxure BMS Server is Connected to License Activation Server
  • Adding an Entitlement without the HTML file when an EcoStruxure BMS Server is Connected to License Activation Server
  • Assigning Licenses
  • Activating Licenses Online
  • EcoStruxure BMS Server Licensing on Servers not Connected to Internet Workflow
  • EcoStruxure BMS Server Licensing on Servers not Connected to Internet Workflow