Use the Show Licenses view toolbar to manage licenses.
Button |
Description |
Add Server |
Click to add a field server to the list. |
Assign Licenses |
Click to assign licenses on the selected field server. For more information, see Assign and Activate Licenses . |
Activate |
Click to activate licenses on the selected field servers. For more information, see Assign and Activate Licenses . |
Return |
Click to return licenses on the selected field servers. For more information, see Return Licenses on EcoStruxure BMS Servers . |
Reclaim |
Click to reclaim licenses on the selected field servers. For more information, see Reclaim Licenses . |
Refresh License Status |
Click to refresh the license status on the selected field servers. |
Other |
Click to open the Other menu. For more information, see Other Menu . |
Current state |
Select to view the current status of the activated licenses. |
Edited state |
Select to view the sum of assigned and activated licenses. |
Show licenses |
Select to show the Show licenses view toolbar. |