earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Basic Functionality
10/30/2025

Properties Grid

arrow1_rotationProperty Context Menu

The Properties grid is one of the three ways to access the properties of a selected object in WorkStation. For more information, see Object Properties .

You access the Properties grid of an EcoStruxure BMS object (e.g., alarm, trend log, value) when you navigate in the List view and you want to keep the List view elements visible.

You use the Properties grid to add new properties, edit values, change units or execute any action related to the property of the given object.

 
action_zoom_plus_stroke

Property Context Menu

Use the property context menu to open the menu specific for the given property from the properties list. The content of the property context menu depends on the property you are working with.

For more information, see Property Context Menu .

  • Object Properties
  • Property Context Menu
  • Workspace Components and Customization