earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Trends
12/3/2024

Creating a Multi Trend Log List in WebStation

You create a multi trend log list to display values from multiple trend logs in one list so that you can compare the values.

Show More
action_close

A trend log list displays all values in the trend log in a list.

In the trend log list, you can perform the following tasks:

  • View all the values and their time stamp.

  • Add and edit records, for example if you knew that some records might be wrong or are missing.

  • Export values as an Excel file.

  • Export values as an xml file.

  • View meter log changes.

  • View events.

  • Change the settings.

 
action_zoom_plus_stroke A Trend log list in WebStation
Figure: A Trend log list in WebStation

To create a multi trend log list in WebStation
  1. In WebStation, right-click the trend log.

  2. Click Create trend item and then click Multi trend list .

  3. Click Save .

  4. Type a name for the Multi trend log list .

  5. Click OK .

  6. On the Trend log list toolbar, click the Settings button

     
    action_zoom_plus_stroke
    .

  7. Click Settings .

  8. Click Add .

  9. Browse to, and select, the trend log lists you want to compare.

  10. Click Select .

  11. Click Edit button to configure the trend log list.

  12. Click OK .

  • Trend Log Lists in WebStation
  • Trend Log List View
  • Trend Log List Toolbar in WebStation
  • Opening a Trend Log List
  • Meter Function
  • Managing Meter Replacement