earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Dashboards
10/30/2025

Configuring an Alarm Pareto Chart

You configure an alarm pareto chart to get a graphical representation of alarms represented by bars but also by a cumulative line.

Show More
action_close

An alarm Pareto chart is a graphical representation of alarms represented by bars but also by a cumulative line. An alarm pareto chart gives you a quick overview of the most common causes of alarms.

You can define how many bars you want to display in the chart.

By clicking on a bar in the alarm Pareto chart you can view a list of alarms for that particular bar.

To configure an alarm pareto chart
  1. Right-click the dashboard and click Edit dashboard .

  2. Click Configure or click the Settings button

     
    action_zoom_plus_stroke
    .

  3. In the Alarm Pareto Chart Properties dialog box, in the Column box, select the column you want to display in the chart.

  4. Click the Add filter button

     
    action_zoom_plus_stroke
    if you want to apply a filter on the alarms.

  5. In the Max number of bars add the maximum number of bars you want to display in the chart.

  6. In the Caption box, type a caption.

  7. In the Caption link box, enter a link to an object that is relevant for the heat map.

  8. In the Show Legend box, select True to display the name and color of the alarms in the chart.

  9. I the Bar color box, select a color for the bars.

  10. In Y-axis minimum box, enter the minimum value of the left y-axis.

  11. In Y-axis maximum box, enter the maximum value of the left y-axis.

  12. It the Decimals box, select the number of decimals you want to display.

  13. Click OK .

  • How Dashboards Work
  • Dashboard Widgets
  • Widget Dialog Box – Layout Tab
  • Alarm Pareto Chart
  • Alarm Pareto Chart Dialog Box
  • Adding a Widget to a Dashboard