earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Dashboards
10/30/2025

Configuring an Alarm Sankey Chart

You configure a Sankey chart to get a graphically representation of the alarms.

Show More
action_close

An alarm Sankey chart is used to graphically present a Sankey chart of the alarms in the EcoStruxure BMS.

You can select the alarms column you want to display. You can also apply a filter to select the alarms based on the alarm fields.

By clicking on a flow in the chart you can view a list of alarm details for that particular alarm.

To configure an alarm Sankey chart
  1. Right-click the dashboard and click Edit dashboard .

  2. Click Configure or click the Settings button

     
    action_zoom_plus_stroke
    .

  3. In the Alarm Sankey chart dialog box, in the Column box, enter the columns you want to display in the pie chart.

  4. Click the Add filter button

     
    action_zoom_plus_stroke
    if you want to apply a filter on the alarms.

  5. In the Max number of nodes box, enter the number of nodes you want to display.

  6. In the Caption box, type a caption.

  7. In the Caption link box, enter a link to an object that is relevant for the chart.

  8. In the Show Legend box, select True to display legends in the chart.

  9. In the Decimals box, select the number of decimals to display.

  10. Click OK .

  • How Dashboards Work
  • Dashboard Widgets
  • Widget Dialog Box – Layout Tab
  • Alarm Sankey Chart
  • Alarm Sankey Chart Dialog Box
  • Adding a Widget to a Dashboard