earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Dashboards
12/3/2024

Configuring an Event Pareto Chart

You configure an event pareto chart to get a graphical representation of events represented by bars but also by a cumulative line.

Show More
action_close

An event Pareto chart is a graphical representation where the events are represented by bars but also by a cumulative line. An event pareto chart gives you a quick overview of the most common events.

You can define how many bars you want to display in the chart.

By clicking on a bar in the event Pareto chart you can view a list of events.

To configure an event pareto chart
  1. Right-click the dashboard and click Edit dashboard .

  2. Click Configure or click the Settings button

     
    action_zoom_plus_stroke
    .

  3. In the Event pareto chart properties dialog box, in the Column box, select the column you want to display in the chart.

  4. Click the Add filter button

     
    action_zoom_plus_stroke
    if you want to apply a filter on the events.

  5. In the Period box, select a period.

  6. In the Max number of bars box, select the maximum number of bars you want to display in the chart.

  7. In the Caption box, type a caption.

  8. In the Caption link box, enter a link to an object that is relevant for the chart.

  9. In the Show Legend box, select True to display legends in the chart.

  10. In the Bar color field, select a color.

  11. In Y-axis minimum box, enter the minimum value of the y-axis.

  12. In the Show Period box, select True to display the period as a legend.

  13. In Y-axis maximum box, enter the maximum value of the y-axis.

  14. It the Decimals box, select the number of decimals you want to display.

  15. Click OK .

  • How Dashboards Work
  • Dashboard Widgets
  • Widget Dialog Box – Layout Tab
  • Event Pareto Chart
  • Event Pareto Chart Dialog Box
  • Adding a Widget to a Dashboard