earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Semantic
12/3/2024

Configure EcoStruxure Building Automation System to use Semantic Workflow

Use this workflow to configure EcoStruxure Building Automation system to use semantics.

 
action_zoom_plus_stroke Configure EcoStruxure Building Automation system to use Semantic workflow
Figure: Configure EcoStruxure Building Automation system to use Semantic workflow
Change the password for the Administrator on the semantic database

For security reasons, change the password for the admin user on the semantic database. Changing the password of the admin user on the semantic database helps to protect the database. If the password is not changed the Ecostruxure Building Operation generates a system alarm.

The password for the Admin user on the default GraphDB semantic database is "root".

For more information, see Navigating to the Semantic Database .

Refer to the semantic database documentation.

Configure the Semantic settings

In a default set up you normally do not have to do any changes in the configuration. Changes in the configuration are only done if you want to change the EBO user that connects to the semantic database, use a semantic database on another location than the default location, or change or rename the repository.

For more information, see Configuring the Semantic Settings .

Allowing the user on EcoStruxure BMS to use Semantic

Users in EcoStruxure Building Operation must be allowed to use semantics. This is done on user group level. The group Admin are by default allowed to use semantics.

For more information, see Configuring Semantic Permissions .

  • Semantic Overview
  • Configuring the Semantic Settings
  • Configuring Semantic Permissions