earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Engineering
12/3/2024

Content Type Rules Workflow

Use this workflow to create and organize content type rules to match the names of specific folders or container objects on the EcoStruxure BMS server with a specific content type.

Related information is found in the sections after the flowchart.

Create a Content Type for a Folder or a Container

You create a content type to reuse predefined layouts for folders or other container objects.

For more information, see Creating a Content Type .

Create a Content Type Rule

You create content type rules to match a folder or a container name with the relevant content type.

For more information, see Creating a Content Type Rule .

Edit a Content Type Rule

You edit a content type rule to adjust settings of the rule.

Important:

Editing the content type rule is a necessary step in a content type rule creation process.

For more information, see Editing a Content Type Rule .

Rank the Content Type Rules

You rank your content type rules to determine the execution order in case a folder or a container name matches many rules.

For more information, see Ranking the Content Type Rules  .

Tip:

You can optionally clear content types for folders and other container objects if an old set of content type rules applies to them and you would like to update them.

For more information, see Clearing a Content Type .

  • Content Types
  • Content Type Rules – Basic Tab
  • Content Type Rules - List View
  • Creating a Content Type
  • Creating a Content Type Rule
  • Editing a Content Type Rule
  • Ranking the Content Type Rules 
  • Clearing a Content Type