earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Server, FDP Server
Functionalities: Alarms
12/3/2024

Adding an Attachment to an Alarm using WebStation

You add an attachment, for example a .pdf file or a trend log, to assist the user when diagnosing or solving the problem that caused the alarm.

Show More
action_close

You can add attachments to alarm objects, except System Information alarms. An attachment is a link pointing to an object in the system. When an alarm that has an attachment is triggered, a paperclip icon is displayed in the Alarms pane and Alarm Views. It is also possible to configure the attachment to display when the alarm is going from Normal to Alarm state.

An attachment can be: a voice message, a report, a trend chart, a schedule, a Microsoft Word file, a PDF file, a video recording, or a pop-up window that contains information regarding the alarm.

You can add the same attachment or set of attachments to multiple alarms in a single operation. You can also delete the attachments that belong to multiple alarms in a single operation. If you add an attachment that already has been attached to an alarm, the later attachment is added as a duplicate.

You can open attachments provided that the program or editor associated with the attachment is locally installed on your computer. For example, if the attachment is a PDF file, you can open the file if Adobe Reader or a similar program is installed on your computer.

To add an attachment to an alarm using WebStation
  1. In WebStation, select the alarm.

  2. In the Alarm dialog box, click Attachments .

  3. In the Attachments dialog box, click the Add .

  4. Select the attachment.

  5. Click Select .

  6. Select if you want the attachment to be displayed when the alarm is triggered.

  7. Click Save .

  • Alarm Attachments
  • Alarms Pane and Alarm View
  • Select Object and Property Dialog Box
  • Adding an Attachment to an Alarm
  • Adding an Attachment to Multiple Alarms
  • Copying Attachments to Multiple Alarms
  • Removing an Attachment from an Alarm
  • Removing an Attachment from an Alarm using WebStation
  • Removing Attachments from Multiple Alarms