earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Server, FDP Server
Functionalities: Alarms
10/30/2025

Creating a Checklist using WebStation

You create a checklist to connect it to an alarm, and to guide the user when troubleshooting a triggered alarm.

Show More
action_close

A checklist is a set of steps that guides the user to which action to take when an alarm is triggered. If an alarm goes to normal state, the corresponding checklist is also reset and each step has to be checked again.

Checklists can be voluntary or mandatory. You can force the user to check each step in the checklist before the alarm can be acknowledged.

To create a checklist using WebStation
  1. In WebStation, select an alarm object.

  2. In the alarm dialog box, click User actions .

  3. In the Checklist properties, click the Edit button

     
    action_zoom_plus_stroke
    .

  4. Click the Add button

     
    action_zoom_plus_stroke
    to create a new checklist and then click Add to add a checklist step.

  5. Click Save .

  • Alarm Functions
  • Alarms Overview
  • User Actions
  • Adding a Checklist to an Alarm using WebStation
  • Editing a Checklist using WebStation
  • Configuring Forced User Actions using WebStation