earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Server, FDP Server
Functionalities: Alarms
12/3/2024

Adding a Checklist to an Alarm using WebStation

You add a checklist to an alarm to troubleshoot the problem that triggered the alarm.

Show More
action_close

A checklist is a set of steps that guides the user to which action to take when an alarm is triggered. If an alarm goes to normal state, the corresponding checklist is also reset and each step has to be checked again.

Checklists can be voluntary or mandatory. You can force the user to check each step in the checklist before the alarm can be acknowledged.

To add a checklist to an alarm using WebStation
  1. In WebStation, select the alarm object.

  2. In the alarm dialog box, click User actions .

  3. Click in the Checklist to open the checklist list.

  4. Click on the checklist you want to use.

  5. Click Save .

To add a checklist to an alarm, you must have created one in advance and defined its content.

  • Alarm Functions
  • Alarms Overview
  • Checklists
  • User Actions
  • Configuring Forced User Actions using WebStation
  • Editing a Checklist using WebStation
  • Creating a Checklist using WebStation