earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Device Administrator, FDP Server
Functionalities: Security
2/25/2025

Device Administrator CA Certificate Workflow

Use this workflow to create a trusted chain between Device Administrator and field server using a CA certificate.

 
action_zoom_plus_stroke Device Administrator CA Certificate Workflow
Figure: Device Administrator CA Certificate Workflow
Start the Device Administrator as an Administrator

You need to be an administrator to install the CA certificate in Windows trusted storage. Refer to Windows for information on how to run a program as administrator.

Import the CA root certificate

Import the certificate.

For more information, see Importing an SSL Root Certificate Using Device Administrator .

Install the CA root certificate in Windows trusted storage

Install the SSL root certificate in Windows trusted storage.

For more information, see Installing an SSL Root Certificate to Windows Trusted Root Certificate Storage Using Device Administrator .

Temporarily trust an invalid certificate

Trust the invalid certificate so that Device Administrator can transfer the certificate to the field server.

For more information, see Temporarily Trusting an Invalid Certificate .

Generate an SSL certificate for each field server

Generate an SSL certificate for each field server.

For more information, see Generating an SSL Certificate for a Field Server Using Device Administrator .

If you have many field servers in the list, you can use the Manage SSL Certificate Template to add default values for every new SSL certificate you want to generate.

For more information, see Generating an SSL Certificate for a Field Server Using Device Administrator .

Save the server list

You save the list after you have generated the certificates for each field server. It is recommended that you save the list after that you have generated the certificate for each field server.

Transfer the SSL certificate to the field server

Transfer the SSL certificate to all field servers in the list. This must be done manually for each server.

For more information, see Transferring an SSL Certificate to a Field Server Using Device Administrator .

Tip:

The certificates are included in the field server’s backup. You do not need to generate a new certificate if you restore a field server from a backup generated after the certificate was transferred to the field server if you retain the original root certificate.

  • Certificates Managed using Device Administrator
  • Generating an SSL Root Certificate Using Device Administrator
  • Installing an SSL Root Certificate to Windows Trusted Root Certificate Storage Using Device Administrator
  • Temporarily Trusting an Invalid Certificate
  • Generating an SSL Certificate for a Field Server Using Device Administrator
  • Transferring an SSL Certificate to a Field Server Using Device Administrator
  • Generating an SSL Certificate for a Field Server Using Device Administrator