Use this workflow to reclaim licenses on EcoStruxure BMS servers that are not connected to Internet.
Do not use this workflow if you are on a semi online system where the EcoStruxure BMS servers are not connected to Internet, but the Device Administrator is connected to the Internet.
For more information, see Semi Online System .
You need one computer running Device Administrator that is connected to Internet.
Related information can be found in the sections after the flowchart.
You gather, and download, the license information from the EcoStruxure BMS servers. This information is used to identify the licenses that are to be reclaimed.
For more information, see Gathering Server Information .
You download the license information file to be able to send the information on the licenses that is to be reclaimed.
This step must be done a computer that is connected to Internet.
For more information, see Downloading License Information .
You create request files to get a response file with reclaimed licenses.
For more information, see Creating the Request Files when Reclaiming Licenses .
You upload request files with license information so that you can receive response files that you send to the EcoStruxure BMS server.
This step must be done a computer that is connected to Internet.
For more information, see Uploading Request Files .
You send the response files to the EcoStruxure BMS servers to complete the offline activation of licenses or the offline reclaim of licenses.
For more information, see Sending the Response Files to the EcoStruxure BMS Server when Reclaiming Licenses .