earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Device Administrator, FDP Server
Functionalities: Engineering, License Management
10/30/2025

Return Licenses on EcoStruxure BMS servers not Connected to Internet Workflow

Use this workflow to return licenses when neither Device Administrator nor the EcoStruxure BMS servers are connected to the Internet.

Note:

Do not use this workflow if you are on a semi online system where the EcoStruxure BMS servers are not connected to Internet, but the Device Administrator is connected to the Internet.

You need one computer running Device Administrator that is connected to Internet.

Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Return Licenses on EcoStruxure BMS servers not connected to Internet workflow
Figure: Return Licenses on EcoStruxure BMS servers not connected to Internet workflow
Create the request files

You create request files to get a response file with returned licenses from License Activation Server.

You gather, and download, the license information from the EcoStruxure servers. This information is used to identify the licenses that is to be returned from License Activation Server.

For more information, see Creating the Request Files when Activating Licenses on EcoStruxure BMS Server not Connected to Internet .

Upload request files on License Activation Server to receive response files

You upload request files to License Activation Server with license information so that you can receive response files that you send to the EcoStruxure BMS server.

This step must be done a computer that is connected to Internet and has access to License Activation Server.

For more information, see Uploading Request Files .

Send response files to the EcoStruxure BMS server

You send the response files from License Activation Server to the EcoStruxure BMS server when you want to return licenses.

For more information, see Sending the Response Files to the Selected EcoStruxure BMS Server when Returning Licenses .

Confirm return licenses on License Activation Server

You confirm the return of licenses so that License Activation Server can active the returned licenses again.

This step must be done a computer that is connected to Internet and has access to License Activation Server.

For more information, see Confirming the Return of Licenses on the License Activation Server .

  • Centralized Licensing Overview
  • Creating the Request Files when Activating Licenses on EcoStruxure BMS Server not Connected to Internet
  • Uploading Request Files
  • Sending the Response Files to the EcoStruxure BMS Server when Activating Licenses
  • Confirming the Return of Licenses on the License Activation Server