earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Device Administrator, FDP Server
Functionalities: License Management
10/30/2025

Semi Online System

A special case is semi online system where the EcoStruxure BMS server is not connected to Internet, but Devices Administrator is connected to internet.

A semi online system contains two parts.

  • A network with EcoStruxure BMS servers. This network cannot connect to Internet and have no possibility to access License Activation Sever.

  • A computer running Device Administrator that is connected to Internet and have access to License Activation Server. This computer can also connect to at least one of the field servers on the network with the field servers.

A semi online system is treated as online for licensing purposes. If you are using a semi online system, you do not have use the licensing offline workflows.

  • Centralized Licensing Overview
  • Assign and Activate Licenses
  • Return Licenses on EcoStruxure BMS Servers
  • Reclaim Licenses