To get correct values in the consumption monitor, the consumption value in the consumption monitor must be configured to handle for example meter roll over.
The start value of a newly created consumption monitor matches the value of the monitored variable, that is, the physical meter.
You must specify the maximum value of the physical meter in the consumption monitor that tracks the physical meter. When the physical meter rolls over, the consumption monitor will continue to increase the value. If you keep the default value (0) in the consumption monitor, the consumption monitor will enter the mode Action needed when the physical meter rolls over. For more information, see Consumption Monitor Status and Mode .