earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Alarms
12/10/2024

XLSX Reports Workflow

Use this workflow to create and configuring an XLSX report.

For more information, see XLSX Reports Overview .

Related information is found in the sections after the flowchart.

 
action_zoom_plus_stroke XLSX Reports Workflow
Figure: XLSX Reports Workflow
Create the XLSX Reports object

Create the XLSX Report object and open the object.

For more information, see Creating an XLSX Report .

Create and configure the XLSX template

Create and configure the XLSX template

For more information, see Creating and Configuring the XLSX Template .

Adding the context to the XLSX spreadsheet

For more information, see Adding the Context to the XLSX Spreadsheet .

  • XLSX Reports Overview
  • Creating an XLSX Report
  • Creating and Configuring the XLSX Template
  • Adding the Context to the XLSX Spreadsheet