earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Security
10/30/2025

Configuring the Global Certificate Settings

You configure the global certificate settings so that the EcoStruxure Building Operation servers can communicate with the PKI server using EST.

Show More
action_close

Public Key Infrastructure (PKI) involves managing digital certificates, public and private keys, and other security elements across multiple servers.

It provides a framework for secure communication by using asymmetric encryption, where each server has a public-private key pair. The public keys are distributed widely and used to encrypt data, while the private keys are kept secret and used to decrypt the data. This ensures secure data transmission between servers. Additionally, PKI involves certificate authorities (CAs) that issue and verify the authenticity of digital certificates, adding an extra layer of trust to the system.

If your organization has its own Public Key Infrastructure (PKI) this can be used to increase the security of your EcoStruxure Building Operation system.

EcoStruxure Building Operation supports the Enrollment over Secure Transport (EST) protocol.

To configure the global certificate settings
  1. In WorkStation, in the System Tree pane, expand System .

  2. Expand Security Manager .

  3. Click PKI Settings .

  4. Click Properties .

  5. Click the Basic tab.

  6. Configure the settings. For more information, see PKI Settings Dialog Box – Basic Tab .

  7. Click Save .

You can configure multiple servers at the same time using search and mass editing.

For more information, see Search Overview .

For more information, see Mass Editing Objects .

  • Public Key Infrastructure in EcoStruxure Building Operation
  • Configure the Certificate Agent Workflow
  • PKI Settings Dialog Box – Basic Tab
  • Web Server Certificate Dialog Box – Basic Tab
  • Configuring Communication with the Enrollment over Secure Transport Server