earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Builder View
Functionalities: Engineering
12/16/2025

Options Dialog Box – Builder Settings

Use the Options dialog box - Builder Settings to manage exposed properties settings in Builder for Application.

 
action_zoom_plus_stroke Options dialog box - Builder Settings
Figure: Options dialog box - Builder Settings

Table: Options dialog box - builder settings

Component

Description

Edit

Click to edit which canvas object properties preferences you want to expose. For more information, see Preferences: Exposed Properties Dialog Box .

Import

Click to import preferred exposed properties. The imported preferences will be added to your existing saved preferences. For more information, see Preferences: Exposed Properties Dialog Box .

Export

Click to export your existing saved preferred exposed properties to be able to share them with other users. For more information, see Preferences: Exposed Properties Dialog Box .

Reset

Click to remove all your existing saved preferred exposed properties and to reset them back to the original default exposed properties. For more information, see Removing Exposed Properties Preferences .

  • Preferences: Exposed Properties Dialog Box
  • Tools Menu
  • Removing Exposed Properties Preferences