earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WorkStation, WebStation
Functionalities: Basic Functionality, Graphics
6/2/2025

Fire Graphic Menus

arrow1_rotationShow Menu arrow1_rotationStatus Menu arrow1_rotationActions Menu

The graphic menus in EcoStruxure Fire Operation are used to display alarms and alerts in a graphic. The menus are also used to apply commands on either loop devices and zones in a graphic or on the fire detection system.

Show Menu

In WorkStation or WebStation, in a fire graphic, you use the Show menu to display, hide, or search for addresses and zones.

 
action_zoom_plus_stroke Show menu
Figure: Show menu

For more information, see Displaying and Searching for Addresses and Zones in a Graphic .

Status Menu

In WorkStation or WebStation, in a fire graphic, the Status menu displays number of active alarms and alerts in categories such as alarms, faults, and disablements. The category color is used in the graphic on loop devices and zones having the same status as the category.

 
action_zoom_plus_stroke Status menu
Figure: Status menu

Actions Menu

In WorkStation or WebStation, in a fire graphic, you use the Actions menu to disable, enable, or request an address update on a loop device or a zone in the graphic. By executing system commands, you affect different categories of alarms and alerts in the entire fire detection system.

 
action_zoom_plus_stroke Actions menu
Figure: Actions menu

For more information, see Disabling Loop Device or Zone in a Graphic .

For more information, see Enabling Loop Device or Zone in a Graphic .

For more information, see Requesting Address Update on Loop Device or Zone in a Graphic .

For more information, see Executing System Commands on Fire Detection System from a Graphic .

  • How Graphics Work in Fire Operation