You use graphics to display building overviews, display the status of detectors and alarms, display the value of sensors, or change setpoints. A graphic can also contain links to trend charts, trend log lists, Internet sites, or views in WorkStation and WebStation.
A graphic that contain links to documents, such as Microsoft Word or Adobe PDF, can be opened in WorkStation and WebStation. The associated programs, in this case Microsoft Word or Adobe Reader, has to be installed on the computer running WorkStation or WebStation.
If a default graphic is defined in the fire detection system configuration, the Home button
If a navigation menu is created in the fire detection system configuration, the Navigation button
The graphic menus in EcoStruxure Fire Operation are used to display alarms and alerts in a graphic. The menus are also used to execute commands on loop devices and zones, or on the fire detection system.
For more information, see Graphic Menu Components .
There are three sets of icons in fire graphics: default icons, Swedish icons, and Finnish icons. In Fire Expert Graphics manager, you choose which icon set you want the graphics to use.