earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation, WebStation
Functionalities: Basic Functionality, Graphics
6/2/2025

Executing System Commands on Fire Detection System from a Graphic

You use the Actions menu to execute system commands on the fire detection system.

Executing a system command affects the entire fire detection system, not only what is displayed in the graphic.

To execute system commands on a fire detection system from a graphic
  1. In WorkStation or WebStation, in a fire graphic, in the Actions menu, click the system command button

     
    action_zoom_plus_stroke
    .

  2. To execute reset commands, click the Reset button

     
    action_zoom_plus_stroke
    and then select the command you want to execute.

    For more information, see Commands .
  3. To execute silence commands, click the Silence button

     
    action_zoom_plus_stroke
    and then select the command you want to execute. For more information, see Commands .

  4. To execute re-sound commands, click the Re-sound button

     
    action_zoom_plus_stroke
    and then select the command you want to execute. For more information, see Commands .

  5. Click the Apply button

     
    action_zoom_plus_stroke
    to execute the command.