earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Server, FDP Server, WorkStation
Functionalities: Basic Functionality
12/3/2024

Actions Menu – Advanced Submenu

Use the Advanced submenu to peform advanced operations, such as repairing communications or references.

 
action_zoom_plus_stroke The Actions menu - Advanced submenu
Figure: The Actions menu - Advanced submenu

Command

Description

Add attachment

Click to add an alarm attachment to one or several alarms.

Clear Content Type

Click to clear a content type applied on a folder or container object. For more information, see Content Types .

Copy attachments from

Click to copy alarm attachments from one alarm to one or several other alarms.

Detect Subnet/Node conflicts

Click to detect address conflicts in the network. The command finds and presents the neuron IDs of any online devices that share the same subnet/node address.

Repair references

Click to repair references when you have moved, renamed, or deleted an object that refers to another object that is offline. For more information, see Copy, Paste, Duplicate, Move, Rename, and Delete .

Repair server communication

Click to repair server communication after an EcoStruxure BMS server has been offline. For more information, see Repairing EcoStruxure BMS Server Communication .

Rebind

Click to rebind a LonWorks network and clear and recreate all LonWorks bindings.

Remove all attachments

Click to remove all alarm attachments from one or several alarms.

Select Content Type

Click to select a content type that you want to apply to a folder or container object. For more information, see Content Types .

Copy properties from…

Click to choose the object that you want to copy properties from.

Change Control

Click to open the Change Control submenu. For more information, see Actions Menu – Change Control Submenu .

  • Copy, Paste, Duplicate, Move, Rename, and Delete
  • Actions Menu
  • Repairing EcoStruxure BMS Server Communication
  • EcoStruxure BMS Server Status
  • Adding an Attachment to Multiple Alarms
  • Copying Attachments to Multiple Alarms
  • Removing Attachments from Multiple Alarms
  • Mass Copying Selected Properties
  • Content Types
  • Select Content Type Dialog Box
  • Actions Menu – Change Control Submenu
  • Change Control