earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Basic Functionality
10/30/2025

Select Object and Property Dialog Box

Use the Select Object and Property dialog box to select an object and its properties.

 
action_zoom_plus_stroke Select object and Property dialog box
Figure: Select object and Property dialog box

Table: Select Object and Property Dialog Box

Component

Description

Lock path

Select to lock the path and make it absolute. For more information, see Locked and Unlocked Binding Paths .

Path

Displays the path to the selected object.

  • Locked and Unlocked Binding Paths
  • Select Object Dialog Box