earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Localization
12/3/2024

Add or Remove Languages Dialog Box

Use the Add or remove languages dialog box to add or remove language that can be selected in WebStation.

 
action_zoom_plus_stroke Add or remove languages dialog box
Figure: Add or remove languages dialog box

Table: Add or Remove Languages Dialog Box

Component

Description

Upload new language

Click to add a language to the list. For more information, see Language Packages .

Remove

Click to remove the selected language. For more information, see Language Packages .

  • Language Packages