earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation
Functionalities: Alarms
12/3/2024

Adding a Cause Note to an Alarm

You add a cause note to an alarm to let others know what caused the alarm.

Show More
action_close

A cause note is a predefined note that contains information on what triggered the alarm. This information can be helpful the next time the same alarm is triggered.

In some cases, adding a cause note is optional. In other cases, you are required to add a cause note when you acknowledge the alarm. 

You add a cause note using WorkStation or WebStation. You can view a cause note added to an alarm in WorkStation or Webstation.

To add a cause note to an alarm
  1. In WorkStation, in the Alarms pane, right-click the alarm and then click Add cause note .

  2. In the Cause Notes dialog box, select the cause note.

  3. Click OK .

The cause note is added to the alarm.

  • Cause Notes
  • Viewing a Cause Note
  • Alarms Pane and Alarm View
  • Alarms Pane Context Menu
  • Cause Notes Dialog Box
  • Alarms Pane and Alarm View Toolbar