earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation
Functionalities: Alarms
12/3/2024

Adding a Check Mark to a Checklist

You add a check mark to a checklist to show which steps you have completed to solve the cause of the alarm.

Show More
action_close

Checklists are predefined lists with steps you take to correct the cause of the alarm.

In some cases, adding a check mark to a checklist in an alarm is optional. In other cases, you are forced to add a check mark when you acknowledge the alarm.

You add a check mark to a checklist using WorkStation or WebStation. You can view the check marks added to a checklist in WorkStation and WebStation.

To add a check mark to a checklist
  1. In WorkStation, in the Alarms pane, right-click the alarm and then click Checklist .

  2. Select the steps you have completed.

  3. Click OK .

The steps in the checklist are added to the alarm.

  • Checklists
  • Viewing a Checklist
  • Alarms Pane and Alarm View
  • Alarms Pane Context Menu
  • Alarms Pane and Alarm View Toolbar