earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Schedules
12/3/2024

Adding a Weekly Event

You add weekly events to a schedule to determine when the event is to regularly occur. Weekly events always occur regularly unless overridden by an exception event.

Show More
action_close

A weekly event occurs every week for an extended period of time on a regular basis. You can schedule more than one weekly event for each day of the week.

To add a weekly event
  1. In WebStation, in the System Tree pane, select the schedule you want to add the weekly event to.

  2. In the Schedule toolbar, click Add weekly event , and select the week day.

  3. In the Weekday dialog enter the start time and the end time or select All day .

  4. In the Value box , enter the value.

  5. Click OK .

  6. Click Save .

  • Weekly Events in WebStation
  • Exception Events in WebStation
  • Schedule Editor in WebStation
  • Schedule Workspace
  • Schedule Event Properties Dialog Box – Weekly View
  • Editing a Weekly Event
  • Editing the Start Time and End Time for a Schedule Event
  • Adding a Single Date Exception Event
  • Adding a Date Range Exception Event
  • Adding a Calculated Exception Event
  • Adding a Calendar Exception Event