earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Alarms
12/3/2024

Alarm Styles View

Use the Alarm Styles view to open the style properties of the different Alarm states.

 
action_zoom_plus_stroke Alarm Styles view
Figure: Alarm Styles view

Table: Alarm Styles View

Component

Description

Acknowledged Style

Click to select the style object that configures the appearance of an acknowledged alarm in the Alarms pane and Alarm View. For more information, see Acknowledged Style Properties .

Alarm Style

Click to select the style object that configures the appearance of a triggered alarm in the Alarms pane and Alarm View. For more information, see Alarm Style Properties .

Disabled Style

Click to select the style object that configures the appearance of a disabled alarm in the Alarms pane and Alarm View. For more information, see Disabled Style Properties .

Fault Style

Click to select the style object that configures the appearance of an alarm with fault state in the Alarms pane and Alarm View. For more information, see Fault Style Properties .

Reset Style

Click to select the style object that configures the appearance of a reset alarm in the Alarms pane and Alarm View. For more information, see Reset Style Properties .

  • Alarm States
  • Alarms Pane and Alarm View Customization
  • Acknowledged Style Properties
  • Alarm Style Properties
  • Disabled Style Properties
  • Fault Style Properties
  • Reset Style Properties