earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Basic Functionality
12/3/2024

Alarm View Properties

Use the Alarm View properties to configure and view the general and object references properties. For more information, see General Information Properties – Basic Tab .

 
action_zoom_plus_stroke Alarm properties
Figure: Alarm properties

Property

Description

Display on alarm

Select True to to automatically open and display the attachment when the alarm is going from Normal to Alarm state.

Show milliseconds

Select True to display the alarm timestamp in milliseconds.

  • General Information Properties – Basic Tab
  • Alarms Overview