earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server
Functionalities: Basic Functionality
10/30/2025

Archive Formats and Storage

You generate an archive by selecting either a CSV or XML format. You can store the archive in Enterprise Server, Enterprise Central, or define a different location.

Table: Comparison of Archiving Formats

Method

Description

CSV

Comma Separated Values is a standard text file that stores spreadsheet or database information in a simple table format. Each record is on a separate line and each field within that record is separated by a delimiter, such as a comma.

XML

​Extensible Markup Language is a markup language that defines a set of rules for formatting documents. Primarily, XML is used to structure, transport, and store data rather than to display data.

Archive Storage and Validation

You define a path to store the archives on your file system.

The preferred path is to the Archives folder in the Enterprise Server or Enterprise Central:

  • Enterprise Server: ..\ProgramData\Schneider Electric EcoStruxure\Building Operation <version>\Enterprise Server\db

  • Enterprise Central: ..\ProgramData\Schneider Electric EcoStruxure\Building Operation <version>\Enterprise Central\db

You can use another location, such as a network drive or external memory device. To ensure that the new location is valid, you can prompt the system to validate the path. For more information, see Enabling the Archiving Function and Defining the Archive Folder .

  • Archiving Overview
  • Enabling the Archiving Function and Defining the Archive Folder