earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation
Functionalities: Alarms
10/30/2025

Assigning an Alarm

You assign an alarm to another user and define the time the user has to respond before the alarm is automatically rejected.

Show More
action_close

When you acknowledge an alarm, you let other users know that you have seen the alarm. Acknowledging an alarm does not necessarily mean that you are responsible for solving the cause of the alarm.

When you acknowledge an alarm the color of the alarm in the Alarms pane changes. In WebStation the alarm symbol also changes.

An acknowledged alarm does not disappear from the Alarms pane list.

You can acknowledge one alarm or many alarms at the same time.

To assign an alarm
  1. In WorkStation, in the Alarms pane , right-click the alarm and then click Assign .

  2. In the Assign dialog box, browse to the user or group you want to assign the alarm to.

  3. Select Amount of time until automatically rejected and then type the amount of time you want the alarm to be rejected after.

  4. Click OK .

  • How Alarms Work
  • Assign Dialog Box
  • Alarm Assignments
  • Alarms Pane and Alarm View
  • Alarms Pane Context Menu