Use the Backup and Restore Manager to supervise the backup settings in the EcoStruxure Building Operation software. You can also open this view in any EcoStruxure BMS server to view current and past backup information.
|
Component |
Description |
|
Status |
Displays the current backup status, such as backing up. |
|
Last backup |
Displays the date and time of the last successful backup. |
|
Backup sets path |
Displays the path to where the Enterprise Server stores all EcoStruxure BMS server backups. |
|
Enable Field Server purge |
Select to enable the Enterprise Server to purge the oldest backup of the field server automatically when a new backup for that field server is stored. |
|
Number of Field Server backup sets to store |
Enter the maximum number of backups that the Enterprise Server can store for each field server. |
|
Enable purge of local backup sets |
Select to enable the Enterprise Server to purge the oldest backup automatically when a new backup is stored. |
|
Number of local backup sets to store |
Enter the maximum number of backups that the system can store for the Enterprise Server. |