earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Basic Functionality
12/3/2024

Backup Rules View

Use the Backup rules view to add, edit, or remove backup rules. You can also modify the backup schedule associated with the backup rule. In addition, you can select a backup rule that can act as a lead rule.

 
action_zoom_plus_stroke Backup rules view
Figure: Backup rules view

Table: Backup Rules View

Number

Description

 
action_zoom_plus_stroke

Use the Backup Rules toolbar to create, edit, or remove backup sets. For more information, see Backup Rules Toolbar .

 
action_zoom_plus_stroke

Use the Backup Rules list to modify backup schedules or set up lead rules. For more information, see Backup Rules List .

  • Backup Rules Toolbar
  • Backup Rules List