earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Trends
12/3/2024

Change of Value Trend Log Properties – Basic Tab

Use the Basic tab to configure the Change of value trend log.

 
action_zoom_plus_stroke Change of value trend log properties - Basic tab
Figure: Change of value trend log properties - Basic tab

Table: Change of Value Trend Log Properties - Basic Tab

Property

Description

Status

Displays the status of the trend log.

Enabled

Displays True if the trend log is enabled.

Logged variable

Enter the variable that you want to log.

Delta

Select the minimum value change that triggers a new record.

Activation variable

Enter the variable that makes the trend log start recording values when the variable is True .

For more information, see Trend Log Activation .

Activation time

Specify the time when the trend log is to start recording values.

For more information, see Trend Log Activation .

Maximum log interval

Select the maximum time that can pass between two recordings regardless if the delta value has been exceeded or not.

Log size

Select the number of records to store before old records are overwritten, including internal records generated by the trend log.

For more information, see Log Record Storage .

Clear when enabled

Select True to clear the trend log when it is enabled.

  • Change of Value Trend Logs
  • Trend Log Types
  • Configure Dialog Box – Configuration Tab
  • Trend Log Activation
  • Configure Dialog Box – Operation Tab
  • Log Record Storage
  • Trend Log Does Not Start Record Due to the Start Condition
  • Missing Trend Log Records
  • General Information Properties – Basic Tab
  • References Tab