earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Schedules
10/30/2025

Editing the Start Time and End Time for a Schedule Event

You edit the start time and end time for a schedule event when the condition changes. You can edit the start time for weekly events and single date exception events.

Show More
action_close

A weekly event occurs every week for an extended period of time on a regular basis. You can schedule more than one weekly event for each day of the week.

To edit the start time and end time for a schedule event
  1. In WebStation, in the System tree pane, select the schedule with the event you want to edit.

  2. In the Schedule workspace, click the schedule event you want to edit.

  3. In properties dialog box, in the At box, enter the start time.

  4. In the Until box, enter the end time.

  5. Click OK .

  6. Click Save .

  • Weekly Events in WebStation
  • Exception Events in WebStation
  • Schedule Workspace Toolbar
  • Schedule Editor in WebStation
  • Editing a Weekly Event
  • Editing a Single Date Exception Event
  • Schedule Workspace
  • Schedule Event Properties Dialog Box – Weekly View
  • Schedule Event Properties Dialog Box – Single Date Exception View