earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Basic Functionality
12/3/2024

Checking the Backup Status of an EcoStruxure BMS Server

You check the backup status of an EcoStruxure BMS server to view its backup status and note the date and time of the last backup.

Show More
action_close

Backup Status displays the statuses of an EcoStruxure BMS server: Ready, Backing up, or Backup succeeded.

If a backup does not succeed, the system displays a default alarm informing you of the backup or EcoStruxure BMS server issue. For more information, see Backup and Restore Alarms .

To check the backup status of an EcoStruxure BMS server
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Backup and Restore Manager .

  4. View the EcoStruxure BMS server backup status or date and time of the last successful backup.

  • Backup Status
  • Control Panel Tab
  • Backup and Restore Manager on the Enterprise Server
  • Backup and Restore Manager on a Field Server
  • Checking the Online Status of the Field Server