You configure the properties of an interval trend log to meet the unique needs of your site.
In WorkStation, in the System Tree pane, click the interval trend log you want to configure.
On the File menu, click Properties .
In the properties dialog box, click the Basic tab.
Edit the basic properties:
|
Property |
Description |
|
Status |
Displays the status of the trend log. |
|
Enabled |
Displays True if the trend log is enabled. |
|
Logged variable |
Enter the variable you want to log. |
|
Delta |
Select the minimum value change that triggers a new record. For more information, see Interval Trend Log Delta . |
|
Activation variable |
Enter the variable that makes the trend log start recording values when the variable is True . For more information, see Trend Log Activation . |
|
Activation time |
Specify the time when the trend log is to start recording values. For more information, see Trend Log Activation . |
|
Interval |
Type how often to log the variable. The interval defines the time between two log records. |
|
Log size |
Select the number of records to store before old records are overwritten, including internal records generated by the trend log. For more information, see Log Record Storage . |
|
Clear when enabled |
Select True to clear the trend log when it is enabled. |
Click the Meter Info tab.
Edit the meter properties:
|
Property |
Description |
|
Is meter log |
Select True if the trend log meter function is active. For more information, see Meter Function . |
|
Meter change time |
Enter the time when the meter was changed. |
|
Meter change user |
Enter the name of the user account that changed the meter. |
|
End time |
Enter the time when the old meter was replaced. |
|
End value |
Enter the value the old meter had when it was replaced. |
|
Start time |
Enter the time when the new meter was installed. |
|
Start value |
Enter the value of the new meter when it was installed. |
|
Meter constant |
Enter the constant of the new meter. If the meter counts in kilo (10 3 ), the constant is 1000. |
|
Min value |
Enter the first value of the new meter after roll-over. |
|
Max value |
Enter the last value of the new meter before roll-over. |
Click OK .