earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Alarms
12/3/2024

Configuring the Priority of an Alarm

You configure the priority level of the different alarm states ​to ​meet the unique needs of your site.

To configure the priority of an alarm
  1. In WorkStation, in the System Tree pane, select the alarm you want to configure.

  2. In the properties pane, click the Presentation tab.

  3. ​Under Priorities , select the Same priority check box to enter the same priority.

  4. In the Priorities boxes, enter the priority for each alarm state.

  5. In the Changes have been made dialog box, click Yes to save the changes.

  • Create Alarm Wizard – Presentation Page
  • Alarm Priority