earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Basic Functionality
12/2/2024

Saving a Field Server Backup Set to Another Location

You save a backup set from a field server to another location so you can store the backup set on, for example, a network drive or a USB memory.

To save a Field server backup set to another location
  1. In WorkStation, on the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the EcoStruxure BMS server.

  3. Click Backup Sets .

  4. In the List View , open the Local folder for a field server or the AS Archives folder for an Enterprise Server.

  5. If connected to the Enterprise Server, open the field server folder that contains the backup set.

  6. Select the backup set that you want to save to a different location.

  7. On the Actions menu, click Save To .

  8. In the Save As dialog box, enter a storage location and click Save .

  9. Click Close .

  • Backup Sets
  • Control Panel Tab
  • Backup Sets View
  • No Restore Files Display After Backup
  • Importing a Backup Set to Field Server
  • Renamed Field Server Makes Backup Sets Unavailable
  • Cannot Save a Backup File using WorkStation